cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32F303RE support dual motor drive?

Ysiu
Associate II

Hi there, I am using ststem workbench for stm32, cube mx v 5.3 and mcsdk 5.4. I want to develop a dual motor application with stm32f303re. However, after I generate the code and upload it. It cannot connect through the monitor. (Works for single motor). What would be the potential problem? I would be very appreciate and gratful for receiving any of your suggestions.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Ysiu
Associate II

HI for anyone encounter the same problem. I just solved this issue. Before assigning pin in st motor control workbench, please check if the pin really exsist on the chip. If you assign a pin which is doesn't exist, error occurs.

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards