2019-07-26 8:20 AM
Hi there, I am using ststem workbench for stm32, cube mx v 5.3 and mcsdk 5.4. I want to develop a dual motor application with stm32f303re. However, after I generate the code and upload it. It cannot connect through the monitor. (Works for single motor). What would be the potential problem? I would be very appreciate and gratful for receiving any of your suggestions.
2019-07-26 9:16 AM
HI for anyone encounter the same problem. I just solved this issue. Before assigning pin in st motor control workbench, please check if the pin really exsist on the chip. If you assign a pin which is doesn't exist, error occurs.
2021-06-22 1:20 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards