2026-05-04 1:49 AM - last edited on 2026-05-04 1:55 AM by mƎALLEm
hello ST Community,
Is it possible to change the RDP "Read Out Protection" level from level 1 to level 0 without erasing the flash data?
I've currently been able to change the level from RDP level 1 to level 0 for Nucleo-H755ZI-Q, but changing the level causes a mass erase of the flash drive. Is it possible to avoid this? If so, is there a code example?
Thanks for your support.
Solved! Go to Solution.
2026-05-04 1:53 AM
Hello,
Definitely not possible. It's a protection to prevent reading the flash content after protecting it. Otherwise, it doesn't make sense to make the content readable after regression.
2026-05-04 1:53 AM
Hello,
Definitely not possible. It's a protection to prevent reading the flash content after protecting it. Otherwise, it doesn't make sense to make the content readable after regression.
2026-05-05 2:13 AM
hello @mƎALLEm,
Thanks! Actually, that's not possible. A solution in my case could be to use the PCROP Protection option only for sector 0 of the FLASH.