2019-12-03 6:42 AM
Hy there,
I would like to ask you, if there is possible to get the basic source code that you are uploading to the STM32G431CB ? I am using it with that basic code, with a MOTOR PROFILER GUI. I am trying to change the motor rotation periodicly (eg. after 3 period the direction of the rotation should change IMMIDIATELY) but with the help of the GUI it changes very slow... I would like to modify the code, I just do not know, which code should I download?
Can you please send me the basic source code for STM32G431CB , motor rotation?
Thank you in advance,
N
2021-06-27 9:41 PM
Dear @NN.2y
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards