2021-07-12 7:28 AM
Hi ST Community,
I'm seeking to start a motor with FOC and six-steps to analyze the difference. When i used the FOC example it works fine, but when i change something and download it to the board with Keil the motor control workbench don't connect: Connection failed! No response, check the communication cable...
At least the example BullRunning works, but the 6steps (6S_STEVAL3201_SL_VM) do nothing
What I'm doing wrong?
what i can do to change configurations on the BullRunning and still connect the board to the motor control workbench?
To use 6steps, i need to change something on the board?
2021-07-13 10:07 PM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK).
Best regards