cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure the temperature sensing with build-in NTC for the FOC-SDK?

MS.13
Associate

Hello,

IPM module STGIPQ3H60T has build-in NTC.

How to configure the temperature sensing with build-in NTC for the FOC-SDK?

Thank you,

Mani

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Laurent Ca...
Lead II

Dear @MS.13​ 

I changed your question title and move it to the question text description.

Best regards

Laurent Ca...
Lead II

Dear @MS.13​ 

Welcome to the STM32 Community

Could you give more details to the STM32 Community about your setup?

That is to say the material you use (HW and also SW): CPU(s), board(s), motor(s), tools and versions, and so on.

And more especially did you use STM32 MC tools and what version of those tools you use (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?

Please do not forget to also indicate the compilation tools suite you use (with the version number).

Best regards