cancel
Showing results for 
Search instead for 
Did you mean: 

Can ST-Motor Control Workbench be used without a powerboard and motor ?

CBald.1
Associate II

Hi,

I am interested in making a program for an FOC controlled BLDC motor using the ST Motor Control Workbench (X-CUBE-MCSDK). Currently, I have no motor or powerboard at my disposal due to the quarentine. Is it possible to develop a program in workbench for a Nucleo-64 G474RE board without a powerboard or a BLDC ? Your help would be really appreciated.

4 REPLIES 4
CBald.1
Associate II

Does anyone know if this can be done ?

Claire O.
ST Employee

dear CBald.1,

Do you have at least the Nucleo-64 G474RE board?

I think you can develop code without problem. The problem will be to test the system... (no spinning motor..)

Best regards,

Claire

Laurent Ca...
Lead II

Dear @CBald.1​ 

Do you have still this problem to solve?

And just in case, if not, do not hesitate to share the final solution you found.

Best regards

Laurent Ca...

Laurent Ca...
Lead II

Dear @CBald.1​ 

I guess you don't have to solve this problem anymore, therefore I consider this thread closed.

If not, feel free to reopen it by posting an answer.

Best regards

Laurent Ca...