cancel
Showing results for 
Search instead for 
Did you mean: 

Board Designer permitted crystal clock sources

JoshS
Associate

Using Workbench 6.3.0.

Creating an "inverter" board for a custom board which uses a 25MHz crystal. Only 8, 24, and 48 MHz crystals are offered in the dropdown. 

Can I edit JSON file to "clocksource": "25_crystal"? If not can I edit the CubeMx clock? Can MCSDK firmware be made to work correctly with a 25MHz clock?

0 REPLIES 0