2023-11-03 02:08 AM
Hi,
I made some temperature measures on STSPIN32G4 using a thermal camera.
I saw that the central part 3x3mm of the STSPIN reaches about 70°C, while the sorrounding part does not go beyond 50°C.
My question is the following: if I use the internal temperature sensor I will read the temperature of the central part or the sorrounding part?
Thank you
Federico
Solved! Go to Solution.
2023-11-15 02:53 AM
Hello @FedericoHW and welcome to the ST Community.
I confirm that the internal temperature sensor reports the temperature of the device central part.
2023-11-15 02:53 AM
Hello @FedericoHW and welcome to the ST Community.
I confirm that the internal temperature sensor reports the temperature of the device central part.