Skip to main content
Marc1
Associate III
May 10, 2023
Question

B-G431B-ESC1 Motor Profiler "Over Voltage"

  • May 10, 2023
  • 1 reply
  • 1378 views

I'm using ST Motor Pilot V1.1.5 with eval board B-G431B-ESC1.

Motor: IBL-100SW-1 http://www.itomotor.com/product/detail/67.html

Motor Profiler Configuration:

Pole Pairs: 3

Max Speed: 2000 RPM

Max peak current: 5 A

Magnetic: I-PMSM

ld/Lq: 1

After starting the profiler, the motor tries to start. But then, after a few seconds the profiler stops and shows the fault message "Over Voltage". This happens even if supply voltage is only 12 V. The oscilloscope shows that PWM peak voltage starts with 12 V and then rises up until more than 30 V between GND and motor phases.

This topic has been closed for replies.

1 reply

ST Employee
August 22, 2023

Hello @Marc1 ,
I would be happy to help you if you still need. Have you tried with the latest version of MCSDK 6.1.2. If not, have you tried lowering the amperage on the profiler?
Regards

"If you agree with my answer, please accept it by clicking on ""Accept as solution""."
Marc1
Marc1Author
Associate III
August 28, 2023

Hello @Zied b.,
I used the latest version of MCSDK at that time. It was MCSDK 6.1.1. I have tried lowering current and voltage.

ST Employee
August 28, 2023

Hello @Marc1 
We made some changes on 6.1.2 can you try and tell me if it works better?

Regard

"If you agree with my answer, please accept it by clicking on ""Accept as solution""."