cancel
Showing results for 
Search instead for 
Did you mean: 

ACIM firmware stm32?

ionutF
Associate III
Posted on June 04, 2014 at 14:09

In  UM1052(STM32F0x/F100xx/F103xx/F2xx/F30x/F4xx 

PMSM single/dual FOC SDK v3.4)  it is written:

''Motor Control Software Development Kit (STSW-STM32100) 

designed for and to be used with STM32F0x/F100xx/F103xx, STM32F2xx, 

STM32F302xB/C, STM32F303xB/C and F4xx microcontrollers.The software library 

implements the Field Oriented Control (FOC) drive of 3-phase Permanent Magnet 

Synchronous Motors (PMSM), both Surface Mounted (SM-PMSM) and Internal (I-PMSM). 

The control of an AC induction motor equipped with encoder or tacho generator is described 

in the UM0483 user manual.

But looking in UM0483  (STM32F103xx

AC induction motor IFOCsoftware library V1.0) I have discovered that this pdf uses a different library from the one used in UM1052. 

I have only downloaded from ST.com STM32 PMSM FOC LIB v3.4 WEB ; which has a folder structure different form the one described in UM0483  .

I searched for STM32 FOC Firmware Libraries v1.0 which has ACIM control methods but in vain . 

Can someone tell me if the firmware intitled ''STM32 PMSM FOC LIB v3.4 WEB '' can controll ACIM motors? 

And where is the other library ''STM32F103xx AC induction motor IFOC software library V2.0 '' ??? 

The same  UM1052 says I can find it on st.com, but I can't find it.

4 REPLIES 4
Gigi
ST Employee
Posted on July 01, 2014 at 08:55

Ciao ionut.fasoola

The STM32 PMSM FOC Lib as stated in the name is only of permanet magnet motor (PMSM = pemanent magnet syncronous motors).

Unfortunately the STM32F103xx AC induction motor IFOC software library V2.0 is no more in the web so if you require it you have to ask directly to your nearest ST local support.

Thank you for your report, now the documentation has been updated.

Ciao

Gigi

ionutF
Associate III
Posted on July 04, 2014 at 16:56

Thanks for your reply,Gigi

Another question : is there a library for AC induction motors control using STM32?

Best regards

Gigi
ST Employee
Posted on July 14, 2014 at 10:57

Ciao ionut.fasoola

At the moment the only FW is the STM32F103xx AC induction motor IFOC software library V2.0 and as discussed you have to ask directly to your nearest ST local support.

Ciao

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards