cancel
Showing results for 
Search instead for 
Did you mean: 

使用ST Motor Contorl Workbench 生成工程文件报错

Lzj111111
Visitor

我现在使用P-NUCLEO-IHM001电机上遇到了点问题,stm32cube是6.10版本,X-CUBE-MCSDK是5.4.8版本,生成文件时出现了如图所示的问题。该怎么解决

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @Lzj111111,

The language of the Community is English as mentioned here.

Refer to the MCSDK5.4.8 release note for the STM32 environment. You must first install STM32CubeMX v6.4.0 and the expected STM32Cube_FW_F3_V1.11.3 firmware package (in your image, it is mentioned as expected but not installed).

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

2 REPLIES 2
GMA
ST Employee

Hello @Lzj111111,

The language of the Community is English as mentioned here.

Refer to the MCSDK5.4.8 release note for the STM32 environment. You must first install STM32CubeMX v6.4.0 and the expected STM32Cube_FW_F3_V1.11.3 firmware package (in your image, it is mentioned as expected but not installed).

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

我按照你的提示操作后,又出现了如图所示的错误,这又该怎么解决,谢谢