cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-AI.3.4.0 This IP has no parameters to be configured.

max.su
Associate

hi

My STM32cubeMX version is 5.2.0

X-CUBE-AI.3.4.0

But when I follow the steps, I find the information as follows:

0690X000008aH1VQAU.jpg

So what should I do to make it OK?

Br,

Max.Su

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
fauvarque.daniel
ST Employee

The X-Cube-AI STM32CubeMX plugin is not loaded in your environment.

I recommend to uninstall the X-Cube-AI pack and reinstall it.

If the installation is successful you should have this file in your installation: C:\Users\xxxx\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\3.4.0\CubeMX\plugins\ip\ai.3.4.0.jar

Regards


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.