cancel
Showing results for 
Search instead for 
Did you mean: 

System Workbench and Cube-AI build error

Elvar Liiv
Associate

Hello.

I run into a following error while building my project using ai:  

make: *** No rule to make target '/home/user/git/stm32/Drivers/CMSIS/DSP/Source/SupportFunctions/arm_copy_q15.c', needed by 'Drivers/CMSIS/DSP/Source/SupportFunctions/arm_copy_q15.o'. Stop.

Everything else seems to be built nicely, but this one stucks out. As i figured out myself, the arm_copy_q15.c is not located in this subfolder, but the location should be: '/home/user/git/stm32/test_projects/test_board_ai_f767zi/Drivers/CMSIS/DSP/Source/SupportFunctions/arm_copy_q15.c'

Is thre some mistake pathing the file and what can I do to fix it.

I use CubeMX 5.4.0 and CubeAI 4.1.0.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
fauvarque.daniel
ST Employee

Yes it is a bug in the project generation for SW4STM32 introduced AFAIK in CubeMX 5.4.

The workaround is to remove this file from the project and add it again with the correct location

This problem doesn't exist anymore with X-Cube-AI 5.0.0 that will be release by the end of the year. In this release we have decided to embed the DSP files that we need in the AI compiled library.

Regards


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AFraz.1
Associate II

Could you post your entire console output after an attempt to build?