cancel
Showing results for 
Search instead for 
Did you mean: 

X CUBE USB AUDIO not recognized as audio device

Loulou
Associate III

Hello,

 

I want to use X CUBE USB AUDIO examples in X CUBE IDE.

After generating the binary code (without errors) and flashing the binary code via DFU, the card is not recognized as an audio device, I tried on all 4 projects. I unplugged USB, do reset, nothink change.

On the other hand, if I generate for example the binary of another audio project: FP-AUD-SMARTMIC1, and flash it via DFU, the card is recognized as an audio device.

 

Thanks by advance.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
FBL
ST Employee

Hi @Loulou 

You can change your target in the compiler. The only difference is RE with less pin count.

Please consider opening new discussion for further questions.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL