cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I find the source code for the demo in the STM3210e_eval board

PHsi.1
Associate II
1 ACCEPTED SOLUTION

Accepted Solutions
PHsi.1
Associate II

I did find the demo firmware source code under \en.stsw-stm32082\STM3210E-EVAL_FW_V2.1.0 folder.

Thank you very much for your help!!

View solution in original post

5 REPLIES 5
Imen.D
ST Employee

Hello @PHsi.1​ and welcome to the Community :)

You will find the applications of the STM3210E-EVAL board in the STM32CubeF1 MCU package:

STM32Cube_FW_F1_V1.8.4\Projects\STM3210E_EVAL\

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
PHsi.1
Associate II

Thank you. I found the ..\applications and ..\examples sub-folders under ..\STM3210E_EVAL with various project folders, such as ..\ADC...,..\FreeRTOS.. etc.

However, I do not know which project folder contains the source code for the "demo program" that was already installed on the EVAL board

PHsi.1
Associate II

I did find the demo firmware source code under \en.stsw-stm32082\STM3210E-EVAL_FW_V2.1.0 folder.

Thank you very much for your help!!

The original one was definitely part of the SPL rather than HAL libraries.

The HAL / CubeF1 has a broader set of examples.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Ned.
Associate III

Thanks to all; I really find it difficult to find this kind of software.

Cheers, Peter Kelly. ​