2023-01-29 04:35 PM
2023-01-30 11:37 AM
I did find the demo firmware source code under \en.stsw-stm32082\STM3210E-EVAL_FW_V2.1.0 folder.
Thank you very much for your help!!
2023-01-29 11:34 PM
Hello @PHsi.1 and welcome to the Community 🙂
You will find the applications of the STM3210E-EVAL board in the STM32CubeF1 MCU package:
STM32Cube_FW_F1_V1.8.4\Projects\STM3210E_EVAL\
Imen
2023-01-30 07:49 AM
Thank you. I found the ..\applications and ..\examples sub-folders under ..\STM3210E_EVAL with various project folders, such as ..\ADC...,..\FreeRTOS.. etc.
However, I do not know which project folder contains the source code for the "demo program" that was already installed on the EVAL board
2023-01-30 11:37 AM
I did find the demo firmware source code under \en.stsw-stm32082\STM3210E-EVAL_FW_V2.1.0 folder.
Thank you very much for your help!!
2023-01-30 12:27 PM
The original one was definitely part of the SPL rather than HAL libraries.
The HAL / CubeF1 has a broader set of examples.
2023-04-14 07:04 PM
Thanks to all; I really find it difficult to find this kind of software.
Cheers, Peter Kelly.