cancel
Showing results for 
Search instead for 
Did you mean: 

When programming a virgin STM32L4 MCU through dfu-util 0.9, it won't exit dfu mode until power cycle.

BNage.2
Associate II

I am working on a IoT product with the STM32L412CBU6 that requires flashing and testing at our manufacturer. I am able to program the device through DFU mode over USB using:

sudo dfu-util -a 0 -i 0 -s 0x08000000:mass-erase:force:leave -R -D firmware.bin

However, it does not enter back into regular mode. Even if I return the boot pin to low and reset, it still appears as a DFU device with lsusb. However, when I power cycle the device it behaves as if it has the new firmware, and I am able to update the firmware with the exact same script and set it to normal/DFU mode using the boot pin and reset.

My question is why does the dfu update work in EVERY other instance other than the very first time I flash the firmware?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Bob S
Super User

Probably this http://www.efton.sk/STM32/gotcha/g44.html documented by @Community member​  :)

waclawek.jan
Super User
MM..1
Chief III

Why dfutil? STM32Programmer is better for this. And DFU protocol have command for run application , maybe this jump to app work.?

Thanks for the insight. I am going to look into programming the option bytes. It looks like dfu-util has this as an option.

I have to use the DFU protocol because that is the interface we selected in product development for updating firmware. I will investigate if the STM32Programmer can run on arm through the USB.

      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.7.0-RC1
      -------------------------------------------------------------------
 
 
Usage :
STM32_Programmer_CLI.exe [command_1] [Arguments_1][[command_2] [Arguments_2]...]
 
 
Generic commands:
 
 -?, -h, --help         : Show this help
 -c,     --connect      : Establish connection to the device
     <port=<PortName>   : Interface identifier. ex COM1, /dev/ttyS0, usb1,
                          JTAG, SWD...)
    USB port optional parameters:
     [sn=<serialNumber>]   : Serial number of the usb dfu
     [PID=<Product ID>]    : Product ID. ex: 0xA38F, etc, default 0xDF11
     [VID=<Vendor ID>]     : Vendor ID. ex: 0x0389, etc, default x0483
    UART port optional parameters:
     [br=<baudrate>]    : Baudrate. ex: 115200, 9600, etc, default 115200
     [P=<parity>]       : Parity bit, value in {NONE,ODD,EVEN}, default EVEN
     [db=<data_bits>]   : Data bit, value in {6, 7, 8} ..., default 8
     [sb=<stop_bits>]   : Stop bit, value in {1, 1.5, 2} ..., default 1
     [fc=<flowControl>] : Flow control
                          Value in {OFF,Hardware,Software} ..., default OFF
                          Not supported for STM32MP
     [noinit=noinit_bit]: Set No Init bits, value in {0,1} ..., default 0
     [console]          : Enter UART console mode
    JTAG/SWD debug port optional parameters:
     [freq=<frequency>] : Frequency in KHz. Default frequencies:
                          4000 SWD 9000 JTAG with STLINKv2
                          24000 SWD 21333 with STLINKv3
     [index=<index>]    : Index of the debug probe. default index 0
     [sn=<serialNumber>]: Serial Number of the debug probe
     [ap=<accessPort>]  : Access Port index to connect to. default ap 0
     [mode=<mode>]      : Connection mode. Value in {UR/HOTPLUG/NORMAL/POWERDOWN
}
                          default mode: NORMAL
     [reset=<mode>]     : Reset modes: SWrst/HWrst/Crst. Default mode: SWrst
                          Reset mode with UR connection mode is HWrst
     [shared]           : Enable shared mode allowing connection of two or more
                          instances of STM32CubeProgrammer or other debugger
                          to the same ST-LINK probe.
     [tcpport=<Port>]   : Port used for running ST-Link Server, default 7184
    SPI port optional parameters:
     [br=<baudrate>]    : Baudrate.
  1. STM32_Programmer_CLI.exe -c port=usb1 -g