cancel
Showing results for 
Search instead for 
Did you mean: 

What is the correct Vector Table base offset in HAL library STM32Cube FW_H7 V1.10.0 (STM32H730VB)?

DWiśn.1
Associate II

I have two projects: 

·                both on microcontroller STM32H730VB;

·                both created in STM32CubeIDE Version: 1.10.1 with HAL library STM32Cube FW_H7 V1.10.0;

·                HAL version in file stm32h7xx_hal.c: STM32H7xx HAL Driver version number V1.11.0

I want to set Vector Table offset, but one project comment claims “Vector Table base offset field. This value must be a multiple of 0x200.�? when in the other, “Vector Table base offset field. This value must be a multiple of 0x300.�?

I also find information that the “0x300�? version is incorrect: https://github.com/STMicroelectronics/STM32CubeH7/issues/246 but with no confirmation.

I suspect an error at the level of file generation by the Cube, but I need to know which offset value is correct. 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Evangelist III

The ARM v7 RM says: "The Vector table must be naturally aligned to a power of two whose alignment value is greater than or equal to (Number of Exceptions supported x 4), with a minimum alignment of 128 bytes."

To get the "Number of Exceptions supported" take the greatest IRQn in the MCU specific header file. Example for STM32H730: Drivers/CMSIS/Device/ST/STM32H7xx/Include/stm32h730xx.h, TIM24_IRQn = 162). Add to this 16 (the number of special exceptions) and multiply by 4 (sizeof u32).

Round up to a power of two. This gives 0x400.

View solution in original post

4 REPLIES 4
TDK
Guru

It should be a multiple of 0x200 (or maybe 0x400). If you want an official source, you can find it within Cortex-M7 documentation.

Take the size of the vector table and round it up to the nearest power of 2.

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Evangelist III

The ARM v7 RM says: "The Vector table must be naturally aligned to a power of two whose alignment value is greater than or equal to (Number of Exceptions supported x 4), with a minimum alignment of 128 bytes."

To get the "Number of Exceptions supported" take the greatest IRQn in the MCU specific header file. Example for STM32H730: Drivers/CMSIS/Device/ST/STM32H7xx/Include/stm32h730xx.h, TIM24_IRQn = 162). Add to this 16 (the number of special exceptions) and multiply by 4 (sizeof u32).

Round up to a power of two. This gives 0x400.

Try writing/reading SCB->VTOR, should be a bunch of the low order bits STZ (Stuck-at-Zero)

The NVIC substitutes the low order bits to generate a vector load, it doesn't have an adder circuit

Listing say 0x2CC is the end (H723), so 0x400 boundaries

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DWiśn.1
Associate II

Thank you all for your replies and for pointing me to the relevant documentation. I calculated this based on the IRQs number and got 0x400, but the various comments confused me.