2012-12-08 1:19 PM
Subject says it all. Just for clarity if length of my frame is 1024 bytes what should I put into tx buffer: 0x1000(Big Endian) or 0x0010(Little Endian)? I do know that ethernet itself is BE and MCU is LE, so does MAC do the conversion or not?
Thanks. #ethernet-mac2012-12-08 3:08 PM
I'm pretty sure the buffer is sent in byte order, look at some received packets.
Buffer[x+0] = 0x04; Bufer[x+1] = 0x00; 0x1000 = 4096, 0x0400 = 10242012-12-08 3:25 PM
I'm tiered of guessing...I can't do anything because my code doesn't work and I'm trying to figure out why...
So, yes you're correct: 0x0400 = 1024 and if MAC is DUMB-endian (doesn't do conversion) than my code has to convert uint16_t i = 1024(0x0004LE) to 4 (0x0400BE). I'd like to see ANY frame byte by byte to understand MAC actions for every frame field and without guessing!