2024-01-21 07:30 PM
When I add a debug log to the source code, a [version-going-backwards] error occurs.
ERROR: weston-cube-4.0+gitAUTOINC+cd44839e95-r0 do_packagedata_setscene: QA Issue: Package version for package weston-cube went backwards which would break package feeds (from 0:4.0+git0+cd44839e95-r0.1 to 0:4.0+git0+cd44839e95-r0.0) [version-going-backwards]
What should I do so that an error does not occur even if I add a debug log?
2024-04-22 02:10 AM
Hi @kiichi ,
I assume that this question remains without answer because there is not enough details.
If you still facing an issue, could you please provide more details about used firmware and compiler also the steps you followed.
If you have already identified the solution, please share it with our Community. That would be helpful for others.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.