2025-02-08 02:04 AM - edited 2025-02-08 02:20 AM
Hi!
I'm using varadic in C and it seems that when I'm using float with va_args I get HardFault.
I have a runable example here: https://onlinegdb.com/2c6Q1hR-ZB
My question is: Why does I get a hardfault here? How can I solve this? Is there any flags in the compiler I need to configure so I can use float?
matrices[i] = va_arg(args, float*); <--- This gives HardFault
Complete example:
/******************************************************************************
Online C Compiler.
Code, Compile, Run and Debug C program online.
Write your code in this editor and press "Run" button to compile and execute it.
*******************************************************************************/
#include <string.h> /* For memcpy, memset etc */
#include <stdio.h> /* For printf */
#include <stdlib.h> /* Standard library */
#include <math.h> /* For sqrtf */
#include <float.h> /* Required for FLT_EPSILON, FLT_MAX, FLT_MIN */
#include <stddef.h> /* Requried for size_t, NULL etc... */
#include <time.h> /* For srand, clock */
#include <stdarg.h> /* For ... arguments */
void print(const float A[], const size_t row, const size_t column) {
size_t i, j;
for (i = 0; i < row; i++) {
for (j = 0; j < column; j++) {
printf("%0.7f\t", *(A++));
}
printf("\n");
}
printf("\n");
}
void mul(const float A[], const float B[], float C[], const size_t row_a, const size_t column_a, const size_t column_b){
/* Decleration */
size_t i, j, k;
/* Data matrix */
const float* data_a, * data_b;
for (i = 0; i < row_a; i++) {
/* Then we go through every column of b */
for (j = 0; j < column_b; j++) {
data_a = A;
data_b = &B[j];
C[0] = 0.0f; /* Reset */
/* And we multiply rows from a with columns of b */
for (k = 0; k < column_a; k++) {
*C += data_a[0] * data_b[0];
data_a++;
data_b += column_b;
}
C++; /* */
}
A += column_a;
}
}
/*
* Fourth-order Runge–Kutta method.
* Runge-Kutta method is not the best ODE solver, but it's the best ODE solver for fixed step time iteration.
* h - Step time
* Y[iterations*N] - Output
* y[N] - Initial state vector
* N - Dimension for y-vector
* odefun(const float t, float y[], const float* matrices[], const size_t rows[], const size_t columns[])
* ... = const float matrixA[], const size_t rowA, const size_t columnA, const float matrixB[], const size_t rowB, const size_t columnB, const float matrixC[], const size_t rowC, const size_t columnC, etc...
*/
void rk4args(const size_t iterations, const float h, float Y[], float y[], const size_t N, void (*odefun)(float, float*, float**, const size_t*, const size_t*), const size_t number_of_pointers, ...) {
/* Variables */
size_t i, j;
/* Constants */
const size_t length = N * sizeof(float);
/* Create vectors */
float* k1 = (float*)malloc(length);
float* k2 = (float*)malloc(length);
float* k3 = (float*)malloc(length);
float* k4 = (float*)malloc(length);
/* Temporary vectors */
float* yt = (float*)malloc(length);
/* Variables */
float t = 0.0f;
/* Initial output */
memcpy(Y, y, length);
/* Variable arguments */
va_list args;
va_start(args, number_of_pointers);
/* Pointers */
float** matrices = (float**)malloc(number_of_pointers * sizeof(float*));
size_t* rows = (size_t*)malloc(number_of_pointers * sizeof(size_t));
size_t* columns = (size_t*)malloc(number_of_pointers * sizeof(size_t));
/* Get the arguments */
for (i = 0; i < number_of_pointers; i++) {
matrices[i] = va_arg(args, float*);
rows[i] = va_arg(args, const size_t);
columns[i] = va_arg(args, const size_t);
}
/* Perform Runge-Kutta */
for (i = 1; i < iterations; i++) {
/* Receive old output */
for (j = 0; j < N; j++) {
y[j] = Y[(i - 1) * N + j];
}
/* First statement */
memcpy(yt, y, length);
odefun(t, yt, matrices, rows, columns);
for (j = 0; j < N; j++) {
k1[j] = yt[j] * h;
}
/* Second statement */
memcpy(yt, y, length);
for (j = 0; j < N; j++) {
yt[j] += k1[j] / 2.0f;
}
odefun(t + h / 2.0f, yt, matrices, rows, columns);
for (j = 0; j < N; j++) {
k2[j] = yt[j] * h;
}
/* Third statement */
memcpy(yt, y, length);
for (j = 0; j < N; j++) {
yt[j] += k2[j] / 2.0f;
}
odefun(t + h / 2.0f, yt, matrices, rows, columns);
for (j = 0; j < N; j++) {
k3[j] = yt[j] * h;
}
/* Fourth statement */
memcpy(yt, y, length);
for (j = 0; j < N; j++) {
yt[j] += k3[j];
}
odefun(t + h, yt, matrices, rows, columns);
for (j = 0; j < N; j++) {
k4[j] = yt[j] * h;
}
/* Save output */
for (j = 0; j < N; j++) {
Y[i * N + j] = y[j] + (k1[j] + 2.0f * k2[j] + 2.0f * k3[j] + k4[j]) / 6.0f;
}
/* Update t */
t += h;
}
/* Free */
free(k1);
free(k2);
free(k3);
free(k4);
free(yt);
free(rows);
free(columns);
free(matrices);
/* Close */
va_end(args);
}
/* Constants */
#define N 2
#define h 0.1f
#define row_a 2
#define column_a 2
#define row_b 2
#define column_b 1
#define row_u 1
#define column_u 1
#define ITERATIONS 200
/* Create ODE equation */
void odefun(const float t, float y[], float* matrices[], const size_t rows[], const size_t columns[]) {
/* Get the matrices */
float* A = matrices[0];
float* B = matrices[1];
float* u = matrices[2];
/* Get the sizes */
size_t row_A = rows[0];
size_t column_A = columns[0];
size_t row_B = rows[1];
size_t column_B = columns[1];
size_t row_U = rows[2];
size_t column_U = columns[2];
/* Solve y = A*y + B*u */
float Ay[2];
float Bu[2];
mul(A, y, Ay, row_A, column_A, 1);
mul(B, u, Bu, row_B, column_B, 1);
size_t i;
for (i = 0; i < row_A; i++) {
y[i] = Ay[i] + Bu[i];
}
}
int main() {
clock_t start, end;
float cpu_time_used;
start = clock();
/* Declare intial state */
float y0[N] = { 0 };
/* Declare output */
float Y[ITERATIONS * N];
/* Declare number of pointers */
const size_t number_of_pointers = 3;
const float k = 5.0f; /* Spring constant [N/m] */
const float b = 1.4f; /* Damper constant [Ns/m] */
const float m = 2.0f; /* Mass [kg] */
const float F = 8.0f; /* Force [N] */
const float A[row_a * column_a] = { 0, 1, -k / m, -b / m };
const float B[row_b * column_b] = { 0, 1 / m };
const float u[row_u * column_u] = { F };
/* Perform Runge-Kutta 4:th order with extended arguments ... of const float[], const size_t, const size_t etc... */
rk4args(ITERATIONS, h, Y, y0, N, odefun, number_of_pointers, A, (const size_t)row_a, (const size_t)column_a, B, (const size_t)row_b, (const size_t)column_b, u, (const size_t)row_u, (const size_t)column_u);
end = clock();
cpu_time_used = ((float)(end - start)) / CLOCKS_PER_SEC;
printf("\nTotal speed was %f\n", cpu_time_used);
/* Plot */
print(Y, ITERATIONS, N);
return EXIT_SUCCESS;
}
Target: STM32F051R8
2025-02-08 02:15 AM - edited 2025-02-08 02:22 AM
@DMårt wrote:Why does I get a hardfault here?
Have you tried debugging to find out?
Your example shows "Online C Compiler" - do you get the fault in the online compiler? or in real hardware? or both?
Your post doesn't say what target this is on. You've posted under MCUs, but your sig says "STM32MP151AAC3 custom board with STM32-OS as operating system", which is an MPU - not an MCU ?
PS:
You have a lot of malloc() calls, but I don't see any checks that those calls succeed ...
2025-02-08 02:21 AM
Hi! @Andrew Neil
I have updated my question.
My sign is for STM32MP1 series. I've built my own free open source custom board. My question is for a MCU.