cancel
Showing results for 
Search instead for 
Did you mean: 

Using STM32F10x USB device with Windows Vista or Windows 7

peters
Associate II
Posted on July 21, 2011 at 13:57

Hello,

we are using  an STM32F105 as USB device in conjunction with a special

configuration program, that runs on a PC.

If we use a PC with Windows XP, the USB driver is automatically

installed and all works fine.

But if we try the same with a PC running Windows Vista or 7, a driver is NOT

automatically installed and the device is marked as 'not working'.

The only way to avoid this, is a prior installation of the 'dfuSe' package.

After installation of this package, the USB connection works, if you connect

the MCU and the PC.

Is there any other way (for driver installation), without prior installation of

 

the 'dfuSe' package ?

Thanks for all answers !

Regards

moardy

#usb-virtual-com-port #stm32-usb #windows-7 #windows-7 #windows-vista #usb #vcp #usb
16 REPLIES 16
brot-mit-senf
Associate II
Posted on July 29, 2011 at 09:35

THX, you make my day !

tomaszpolus
Associate
Posted on November 02, 2011 at 15:32

How can I make it work with Windows 7 Embedded Standard ?

This is important for me, my application needs WES7. Please help me.

Thank you, Kind Regards,

Tomasz Polus

davidxia9
Associate
Posted on May 31, 2012 at 03:55

Hi, The following link doesn't work

http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/vcpdriver_v1.zip

I found it diffcult to find a useful thing on the internet

http://www.st.com

, I'm very disappointed to ST, they don't really care the customer, what they care is sales, money!

Nickname12657_O
Associate III
Posted on June 01, 2012 at 01:38

Here is the right link :

http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/stm32_vcp.zip

Cheers,

STOne-32.

ben_yong
Associate
Posted on December 26, 2012 at 08:12

Hi, are there any STM32F1 Windows drivers for other USB classes than virtual com port? If yes, can you provide the link to download? Thank you~

nolex90
Associate II
Posted on May 30, 2013 at 13:42

This link is out of date. So, where can I find the VCP drivers?

Posted on May 30, 2013 at 14:10

http://www.st.com/web/en/catalog/tools/PF257938

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..