Using MP45DT02 on STM32F407 Discover board to save data using DMA.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-09 5:31 PM
I am wanting to sample the MP45DT02 microphone data. I am very much a beginner with this but I have cobbled together some code from some examples. Any input as to why I am not able to see any data through the DMA would be greatly appreciated.
DMA_InitTypeDef DMA_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
I2S_InitTypeDef I2S_InitStructure;
SPI_InitTypeDef SPI_InitStructure;
uint32_t ComponentsUsed;
// Enable clocks
ComponentsUsed = RCC_AHB1Periph_DMA1 |
RCC_AHB1Periph_GPIOA |
RCC_AHB1Periph_GPIOB |
RCC_AHB1Periph_GPIOC;
RCC_AHB1PeriphClockCmd(ComponentsUsed, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);
SPI_I2S_DeInit(SPI2);
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Slave;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Hard;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI2, &SPI_InitStructure);
I2S_InitStructure.I2S_AudioFreq = I2S_AudioFreq_48k;
I2S_InitStructure.I2S_Standard = I2S_Standard_Phillips;
I2S_InitStructure.I2S_DataFormat = I2S_DataFormat_16b;
I2S_InitStructure.I2S_CPOL = I2S_CPOL_Low;
I2S_InitStructure.I2S_Mode = I2S_Mode_MasterRx;
I2S_InitStructure.I2S_MCLKOutput = I2S_MCLKOutput_Enable;
I2S_Init(SPI2, &I2S_InitStructure);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_6; // PC pins
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource3, GPIO_AF_SPI2); //I2S2_SD
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_SPI2); // I2S2_MCK
GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_SPI2); // I2S2_WS
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_SPI2); // I2S2_CK
I2S_Cmd(SPI2, ENABLE);
SPI_Cmd(SPI2, ENABLE);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(SPI2->DR);
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)i2s_raw_values_;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 10;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA1_Stream4, &DMA_InitStructure);
DMA_Cmd(DMA1_Stream4, ENABLE);
SPI_I2S_DMACmd(SPI2, SPI_I2S_DMAReq_Rx, ENABLE);
SPI1->CR2 |= SPI_CR2_RXDMAEN;
SPI_I2S_ReceiveData(SPI2);
- Labels:
-
Audio
-
DMA
-
I2S
-
SPI
-
STM32F4 Series