Skip to main content
DDesr.1
Associate II
July 27, 2023
Question

USB PD: Vendor_Defined_Extended Message

  • July 27, 2023
  • 2 replies
  • 2193 views

Hi Community!

We're working with an STM32G0B1xx MCU and using USB PD v5.0.0 library from github (https://github.com/STMicroelectronics/stm32-mw-usbpd-core).

I see here that USBPD_EXT_VDM = 0x1E is defined properly. However, when I use this with USBPD_DPM_SendExtendedMessage(), I get a generic "USBPD_FAIL" response, and nothing gets sent out on the CC line.

So, my question is: Does the v5.0.0 library support Vendor_Defined_Extended message? 

Thank you for the support!

Screenshot from the USB PD 3.1 spec

DDesr1_0-1690487916211.png

 

This topic has been closed for replies.

2 replies

Guenael Cadier
ST Employee
August 2, 2023

Hello @DDesr.1 ,

Do you mean the call to USBPD_PE_SendExtendedMessage() returns USBPD_FAIL ?
If so, it is expected as Vendor_Defined_Extended messages are not supported in v5.0.0 of USBPD Core library.

Regards

DDesr.1
DDesr.1Author
Associate II
August 4, 2023

Hi @Guenael Cadier thank you for responding.

It's too bad.. I could really use the feature :).

Please, let me know if there's anything I can do to help expedite this one .

Thanks again