cancel
Showing results for 
Search instead for 
Did you mean: 

en.x-cube_classb

JWrig.13
Associate

I've downloaded the x-cube_classb application, but none of the projects will build for EWARM

In addition to a few warnings, the linker fails: 

    unable to allocate space for sections/blocks with a total estimated minimum size of 0x220 bytes (max align 0x4) in <[0x2000'0030-0x2000'1fff]> (total uncommitted space 0x1b74).

EWARM version: 9.30.1.50054

Compiler version : 9.30.1.335

    Is this classB code incompatible with this version
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Petr Sladecek
ST Employee

Hello,

as visible from table "STL code size and data size (in bytes)" at user manual, the STL needs ~220 bytes at RAM only. Area 0x2000'0030-0x2000'1fff should be sufficient enough to allocate that. Check your linker file setting (stack/heap size).

Best regards,

Petr

Best regards,

Petr