USB MSC library bug?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-01-13 1:34 PM
Posted on January 13, 2014 at 22:34
Does anyone got USB MSC library working? At least one suspicious place:
File:usbd_msc_scsi.c
(...) static int8_t SCSI_Verify10(uint8_t lun , uint8_t *params){ if ((params[1]& 0x02) == 0x02) { SCSI_SenseCode (lun, ILLEGAL_REQUEST, INVALID_FIELED_IN_COMMAND); return -1; /* Error, Verify Mode Not supported*/ } if(SCSI_CheckAddressRange(lun, SCSI_blk_addr, SCSI_blk_len) < 0) { return -1; /* error */ } MSC_BOT_DataLen = 0; return 0; } /** * @brief SCSI_CheckAddressRange * Check address range * @param lun: Logical unit number * @param blk_offset: first block address * @param blk_nbr: number of block to be processed * @retval status */ static int8_t SCSI_CheckAddressRange (uint8_t lun , uint32_t blk_offset , uint16_t blk_nbr) { if ((blk_offset + blk_nbr) > SCSI_blk_nbr ) ///!!!!!!!! <<< WHAT is here?
{ SCSI_SenseCode(lun, ILLEGAL_REQUEST, ADDRESS_OUT_OF_RANGE); return -1; } return 0; } (...) The first function ''SCSI_Verify10'' calls the later one ''SCSI_CheckAddressRange'' which adds memory address in bytes to number of blocks (typical 1 block = 512 bytes) and compares to maximum number of blocks? May be it should be: if ((blk_offset/ SCSI_blk_size
+ blk_nbr) > SCSI_blk_nbr ) Somebody got this example working? ''SCSI_CheckAddressRange'' function is also used in some other SCSI processings... Addition: After closer look it seems that ''SCSI_Verify10'' is totally wrong (should be similar to Write10). Fixing it ''SCSI_CheckAddressRange'' could be left as is. Anyone from ST could confirm that? #usb-scsi
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0