cancel
Showing results for 
Search instead for 
Did you mean: 

USB Init fails on AHB Idle not set

jim239955
Associate II
Posted on August 29, 2016 at 19:43

STM32F427.

I cloned a cube project for a working application with Micrium os.  I want to run code without an OS.  As far as I can tell so far I am doing all the same initializations but the function USB_CoreReset fails with a return of HAL_TIMEOUT.  (ignored by caller).   USB never becomes operational.  Not that both builds are running on same board.

Anyone have an idea of a string to pull to figure out what's going on?

#usb_corereset #usb #stm32f #ahb
0 REPLIES 0