2021-11-04 9:52 PM
Board name : stm32f746g discovery
I need to update firmware through usb host, i did not get any documents for "stm32f7 series usb host firmware upgrade"
does any one help me ?
For example i need this type firmware upgradation:(it takes from internet)
2021-11-15 6:18 AM
Hello @N Sornakumar ,
You can refer to the following example provided under our F7 CubeFW :
I hope this helps you.
BeST Regards,
Walid
2021-11-16 12:28 AM
Hello @N Sornakumar
Have you tried the example suggested above ?
Please click on Select as Best if my post fully answered your question. This will help other customers with the same issue to find the solution faster!
BeST Regards,
Walid
2021-11-19 2:28 AM
Hello @Walid ZRELLI
. I have an application which is running properly at the starting location i.e
0x0800 0000
(after usb boot)
. If I change the starting location to
0x0800 4000
the application is still running this location 0x0800 0000
So my bootloader not working ??