2011-10-21 10:09 AM
I have successfully detected the microcontroller in the computer but my program and application are not transmitting data through usb. How do i debug the usb connection?
I would be happy if someone would help me providing the parameters to be checked (e.g. clock, endpoint, etc) which would be helpful to track what is the mistake, specially the parameters that are accessible during the debug stages. Thanks in advance. #usb-debug2011-10-21 11:09 AM
http://www.perisoft.net/bushound/
2011-10-24 03:34 AM
Thank you for the application. I used the program but it always showed there is no end point configured but i was able to get the data with hyper terminal and also on my labview application.
Anyway the application was useful in some way and thank you for that.