2014-05-12 3:15 AM
Hello,
I tried virtual COM port example on STM32 and used driver VCP_V1.3.1. I'm surprised that without pre-installing driver the device is found as a composite in Device Manager, and I cannot use the same inf file (attached) as for my old product, based on another ARM and represented a bundle of ACM and CDC interfaces. My problems are: 1) It's not nice to include VCP installer in my own one. But it's a minor problem. 2) VCP_V1.3.1 device is not discoverable by SetupAPI interface (SetupDiEnumDeviceInterfaces() and others). In my old inf I added serenum.sys for that. It's a bigger problem. How can I modify firmware to support custom inf-file, or how can I modify driver to be compatible with SetupAPI? Many thanks Dmitry #vcp #usb #stm322014-05-12 2:40 PM
Hi, Tsuneo!
I've read a lot of your posts about USB-devices and it was very helpfull, thanks for it. May I ask you to help me? My problem is discribed in post: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fCDC%20Host%20for%20STM32F407&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy%2Es...I'll be appriciate for any help.Anthony2014-05-13 1:37 AM
Dear Tsuneo,
Thank you for taking part in the discussion! I don't need to create a composite device. Surprisingly the STM32 VCP without installed drivers is seen as a ''Composite Device'' in Device Manager (and additionally 2 interfaces also are seen in Device Manager as ''Other Devices''). I need that the device behaves the same way as my old device based on LPCUSB VCP. I would send a log from USBlyzer to compare, but LPCUSB device doesn't generate a log without drivers installed.2014-05-13 1:40 AM
Mard's example
behaves the same way.2014-05-13 2:46 AM
We succeeded to use own inf instead of ST driver by adding IAD - interface association descriptor:
USBD_DeviceDesc[USB_SIZ_DEVICE_DESC] __ALIGN_END = { 0x12, /*bLength */ USB_DEVICE_DESCRIPTOR_TYPE, /*bDescriptorType*/ 0x00, /*bcdUSB */ 0x02, 0xEF, //0x00, /*bDeviceClass*/ 0x02, //0x00, /*bDeviceSubClass*/ 0x01, //0x00, /*bDeviceProtocol*/ ............... and then usbd_cdc_CfgDesc[USB_CDC_CONFIG_DESC_SIZ+8] __ALIGN_END = { /*Configuration Descriptor*/ 0x09, /* bLength: Configuration Descriptor size */ USB_CONFIGURATION_DESCRIPTOR_TYPE, /* bDescriptorType: Configuration */ USB_CDC_CONFIG_DESC_SIZ+8, /* wTotalLength:no of returned bytes */ 0x00, 0x02, /* bNumInterfaces: 2 interface */ 0x01, /* bConfigurationValue: Configuration value */ 0x00, /* iConfiguration: Index of string descriptor describing the configuration */ 0xC0, /* bmAttributes: self powered */ 0x32, /* MaxPower 0 mA */ 0x08, // Number Size of this descriptor in bytes. 0x0B, // INTERFACE ASSOCIATION Descriptor 0x00, // Interface number of the first interface that is associated with this function. 0x02, // Number of contiguous interfaces that are associated with this function. 0x02, // Class Class code (assigned by USB-IF). 0x02, // Subclass code (assigned by USB-IF). 0x01, // Protocol Protocol code (assigned by USB-IF). 0x00, // Index of string descriptor describing this function. ............... Then in inf I added &_MI00 after PID. Now inf file is accepted and 2 devices are in Device Manager: 1 x Composite and 1 x Port.2014-05-13 7:07 AM
Thanks for information. Good idea, my congradulations =)
2014-05-15 12:04 AM
Tsuneo was right, suggesting to read Multiple USB CDC (USB IAD). How?
I'm bookmarking it, very useful, thanks again!!