cancel
Showing results for 
Search instead for 
Did you mean: 

USART_SR, clearing sequence of: IDLE, ORE, NF, FE, PE. A silicon level analysis.

elKarro
Associate III

Applies to: STM32L100xx, STM32L151xx, STM32L152xx, STM32L162xx.

Hi,
in order to write robust drivers, I'm kindly asking a few questions to developers who are into the silicon design. This is the 1st:

ref. RM0038 Reference manual Rev 18, paragraph 27.6.1 Status register (USART_SR) vaguely says that error flag(s):
"It is cleared by a software sequence (a read to the USART_SR register followed by a read to the USART_DR register)."

which of the following describes the real case:

0) "It is cleared by a read to USARTx_DR which happens AFTER a read to USARTx_SR, without any other access in between to the USARTx memory space*."

1) "It is cleared by a read to USARTx_DR which happens AFTER a read to USARTx_SR, without any other access in between to the APBx* linked to the USARTx."

2) ???

(*) see 2.3 Memory map - Table 5. Register boundary addresses


Thank you very much in advance.

MCU speaks VHDL and CPU speaks assembly. Neither of them speaks HAL.
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13

> I could rephrase your question as: "why do you think that a read to SR followed by a read to DR will clear the flags?".

That is not a restatement of my question, it's a different question. But the answer is simple: because that's literally what the RM says.

Don't overthink it. Coding is hard enough without hallucinating roadblocks. Cheers.

If you feel a post has answered your question, please click "Accept as Solution".
STea
ST Employee

Hello @elKarro ,

After checking I can confirm that scenario 2 is the right scenario:

2) It is cleared by a read to USARTx_DR which happens AFTER a read to USARTx_SR.

even if other accesses are done in between. it does not matter, and it doesn't matter either if it is done by CPU or DMA.

The state machine of UART needs to detect the sequence as described in RM (a read to the USART_SR register followed by a read to the USART_DR register) things can happen in between and access to the UART address space as well.

BR

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you very much @STea !
Maybe this post clarified that joke you asked me about :- D
Thanks again.

MCU speaks VHDL and CPU speaks assembly. Neither of them speaks HAL.

Hello @elKarro ,

yep, it's clear as your clearing sequence of: IDLE, ORE, NF, FE, PE . :p

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.