2017-01-26 8:04 AM
UART_Printf example (Nucle-F767ZI, 144 pins) works correctly, I get printf output on OS X, using Zterm (PC HyperTerminal replacement).
However mouse is locked when I connect with Zterm and start listening. Computer is thus barely usable, I have to revert to keyboard-mouse accessibility feature (mouse mapped to numerical keys). The same happens with Coolterm, so this is not Zterm specific. Below is the USB-serial device that Zterm selects:
Mouse must be in the same ''channel'' with STM32 in usbmodemFA133. Can ST provide support on this? How to add additional ''usbmodemFAxxx'' driver, separate for STM32 board (Nucleo-F767ZI) ? Internet is blank at this. I think many users can have similar issue.
#freeze #hyperterminal #uart #usb #printf-hal_uart_transmit #os-x #printf2017-01-26 10:46 AM
you dont need zterm or anything. from the shell prompt you can simply
$ screen /dev/tty.usbmodemXXXXXX 115200
your problem is a zterm problem or install problem not a serial port driver problem or stm32 problem.
2017-01-26 3:32 PM
I've did:
screen /dev/tty.usbmodemFA133 9600
and it's the same – mouse is blocked. I kindly ask to include this generic problem in ST support, so that STM32 can print to UART.
2017-01-26 4:01 PM
That's good, it didn't sound reasonable. I am currently working on USB UARTs and just got it working.
My code was generated by cube for the STM32F407G-DISC1 board, so you can regen it for yours (if you wish). All I did was turn on the USB device, device FS, for CDC. Gen the code and then I put in the interface routines for GCC/newlib to use printf/scanf via USB.
Attached is main.c and the support file that has to be munged.
...and the widget to attach a file is gone... what the hell ST????
Sorry about the formatting, I tried but these tools suck.
main.c
...
int
main(void
){
/* USER CODE BEGIN 1 */
/*
* a test program to see what it takes to get a USB
com
port working.*
* To get the I/O to work, I put in the helpers to get stdio to work. This means
* _read and _write.
*
* The USB portion is handled by the code in usbd_cdc_if.c. All of the action happens there.
* Actually, the interface is pretty weird. The only public function is CDC_Transmit_FS. That means
* that there is no access to CDC_Receive_FS externally.
Wuh
?*
* The unwritten interface is that you are supposed to
munge
usbd_cdc_if.c to be able to get at the read* and write routines. So I placed _write in there, which calls CDC_Transmit_FS.
*
* _read is handled a little different. CDC_Receive_FS is a callback routine that is called by the USB stack
* once some data has been received. I ended up putting some code in there to dequeue the USB data and dump
* it into a secondary buffer. Once
getchar
/scanf
/??? is called, _read will then go and attack the secondary* buffer. Of course, _read only returns once the buffering is satisfied, so main calls
setvbuf
to clobber the* stdio buffering.
*
* Since _read is blocking, I also threw in
kbhit
() to free up the processor.*/
char
ch;/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the
Systick
. */HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USB_DEVICE_Init();
/* USER CODE BEGIN 2 */
setvbuf
(stdin, NULL, _IONBF, 0);/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while
(1) {/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
if
(kbhit()) {ch = getchar();
putchar(ch);
}
HAL_Delay(1);
}
/* USER CODE END 3 */
}
usbd_cdc_if.c:
/**
* @brief
CDC_Receive_FS
*
Data received over USB OUT
endpoint
are sent over CDC interface*
through this function.
*
*
@note
*
This function will block any OUT packet reception on USB
endpoint
*
untill
exiting this function. If you exit this function before transfer*
is complete on CDC interface (
ie
. using DMA controller) it will result*
in receiving more data while previous ones are still not sent.
*
* @
param
Buf
: Buffer of data to be received* @
param
Len
: Number of data received (in bytes)* @
retval
Result of the operation: USBD_OK if all operations are OK else USBD_FAIL*/
static
int8_t
CDC_Receive_FS (uint8_t
* Buf,uint32_t
*Len){
/* USER CODE BEGIN 6 */
USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]);
USBD_CDC_ReceivePacket(&hUsbDeviceFS);
receivedLen = *Len;
memcpy
( &receivedData[totalReceived], Buf, receivedLen);totalReceived += receivedLen;
return
(
USBD_OK);
/* USER CODE END 6 */
}
/**
* @brief
CDC_Transmit_FS
*
Data send over USB IN
endpoint
are sent over CDC interface*
through this function.
*
@note
*
*
* @
param
Buf
: Buffer of data to be send* @
param
Len
: Number of data to be send (in bytes)* @
retval
Result of the operation: USBD_OK if all operations are OK else USBD_FAIL or USBD_BUSY*/
uint8_t
CDC_Transmit_FS(uint8_t
* Buf,uint16_t
Len){
uint8_t
result =USBD_OK
;/* USER CODE BEGIN 7 */
USBD_CDC_HandleTypeDef
*hcdc = (
USBD_CDC_HandleTypeDef*)hUsbDeviceFS.
pClassData
;
if
(hcdc->TxState
!= 0){
return
USBD_BUSY;
}
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len);
result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);
/* USER CODE END 7 */
return
result;}
/* USER CODE BEGIN PRIVATE_FUNCTIONS_IMPLEMENTATION */
/**
* @}
*/
int
_write(int
file,char
*outgoing,int
len) {if
(hUsbDeviceFS.dev_state
== USBD_STATE_CONFIGURED){CDC_Transmit_FS( outgoing, len);
}
return
len;}
/**
* @}
*/
int
_read(int
file,char
* result,size_t
len) {if
(len == 0) {
return
(0);}
while
(totalReceived < len) {HAL_Delay(10);
}
memcpy
( result, receivedData, len);totalReceived = 0;
return
(len);}
/**
* @}
*/
bool kbhit(
void
) {return
(totalReceived > 0);}