cancel
Showing results for 
Search instead for 
Did you mean: 

Troubles in connection between STMF4 and a HID device

zaidioussama07
Associate
Posted on December 23, 2016 at 09:31

Hi everyone

This is my first question in this forum, I hope you will not be so agressive with me I am new with microcontrollers.

I am using STM32F407VG discovery as a USB HOST, I connected it to a lazer scanner which reads barcodes, the scanner is considered as a keyboard.

The connection works just fine but I have some issues that I can't define their causes.

First, I can't connect the scanner directly to STM, I need to connect a mouse first, wait until STM  recognize the mouse then I disconnect it and connect the scanner, I don't know why I need to do that but this is the only way to get the scanner connected.

The second issue is that devices take a long time to get connected to STM and some times they don't connect at all, so some times i resolve the problem by take off the supply from STM and putted again, some times i need to run the program again and also I don't know why I need to do that.

So you can imagine if I disconnect the scanner or the STM get off power I need at least 10 minutes to get the connection again.

I did a simple program without interrups,RTOS or using DMA register just I configured the Timer, GPIOs, the USB, I think I have all the files that I need on the library, I don't know the cause of this problem.

This is the code:

&sharpinclude 'defines.h'

&sharpinclude 'tm_stm32f4_usb_hid_host.h'

&sharpinclude 'stm32f4xx.h'

&sharpinclude 'stm32f4xx_rcc.h'

&sharpinclude 'stm32f4xx_gpio.h'

&sharpinclude 'stm32f4xx_tim.h'

&sharpinclude 'misc.h'

&sharpinclude <stdio.h>

uint16_t PrescalerValue, TimPeriod;

int i;

GPIO_InitTypeDef GPIO_InitStructure;

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

TIM_OCInitTypeDef TIM_OCInitStructure;

uint16_t PrescalerValue ;

uint16_t TimPeriod ;

void Timer4_Config(void)

{

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4,ENABLE);

// Te=1s

// TimPeriod*(PrescalerValue+1)/F(timer4)=Te; // F(timer4)=84Mhz

PrescalerValue=8399;

TimPeriod=10000;

TIM_TimeBaseStructure.TIM_Period = TimPeriod ;

TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;

TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);

TIM_Cmd(TIM4 , ENABLE);

}

void GPIO_Config(void)

{

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD,ENABLE );

//Configure LD12---PD15 in output pushpull mode

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12|GPIO_Pin_13|GPIO_Pin_14|GPIO_Pin_15;//LD2...LD15

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;//Mode Out

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;//Fmax=50 MHz

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;//Output Push Pull

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;//No Pull

//GPIOd Periph initialisation

GPIO_Init(GPIOD,&GPIO_InitStructure);

//Connecter chaque pin au TIM4 en mode AF

//void GPIO_PinAFConfig(GPIO_TypeDef* GPIOx, uint16_t GPIO_PinSource, uint8_t GPIO_AF);

}

int main(void) {

TM_USB_HIDHOST_Result_t USB_HID_Status; /* USB HID Host status */

TM_USB_HIDHOST_Keyboard_t tableau [18] ;

/* Initialize system */

SystemInit();

GPIO_Config();//Configuration du GPIO

Timer4_Config();//Configuration du Timer 3

/* Init USB HID */

TM_USB_HIDHOST_Init();

/* Get connected device */

USB_HID_Status = TM_USB_HIDHOST_Device();

while (1)

{

TM_USB_HIDHOST_Process();

USB_HID_Status = TM_USB_HIDHOST_Device();

if ( USB_HID_Status==TM_USB_HIDHOST_Result_KeyboardConnected)

{

for (i=0;i<17;i++)

{

TM_USB_HIDHOST_ReadKeyboard(&tableau[i]);

     if (tableau[i].ButtonStatus == TM_USB_HIDHOST_Button_Pressed) {

          if (tableau[i].Button == '5') {

            if ( tableau[i+1].Button == '1')

               {

                    GPIO_ResetBits( GPIOD, GPIO_Pin_14);

                    GPIO_ResetBits( GPIOD, GPIO_Pin_13);

                    GPIO_ResetBits( GPIOD, GPIO_Pin_12);

                    GPIO_SetBits( GPIOD, GPIO_Pin_15);

                 }

             if (tableau[i+1].Button == '0')

                 {

                     GPIO_ResetBits( GPIOD, GPIO_Pin_12);

                     GPIO_ResetBits( GPIOD, GPIO_Pin_13);

                     GPIO_ResetBits( GPIOD, GPIO_Pin_15);

                     GPIO_SetBits( GPIOD, GPIO_Pin_14); }

                 }

          if (tableau[i].Button == '4') {

             if (tableau[i+1].Button == '1')

                {

                    GPIO_ResetBits( GPIOD, GPIO_Pin_12);

                    GPIO_ResetBits( GPIOD, GPIO_Pin_14);

                    GPIO_ResetBits( GPIOD, GPIO_Pin_15);

                   GPIO_SetBits( GPIOD, GPIO_Pin_13);

                }

             if (tableau[i+1].Button == '0')

                {

                  GPIO_ResetBits( GPIOD, GPIO_Pin_15);

                  GPIO_ResetBits( GPIOD, GPIO_Pin_13);

                  GPIO_ResetBits( GPIOD, GPIO_Pin_14);

                  GPIO_SetBits( GPIOD, GPIO_Pin_12);

                 }

}

if (USB_HID_Status==TM_USB_HIDHOST_Result_MouseConnected)

{

for(i=0;i<4200000;i++)

GPIO_SetBits( GPIOD, GPIO_Pin_15);

for(i=0;i<4200000;i++)

GPIO_ResetBits( GPIOD, GPIO_Pin_15); }

if (USB_HID_Status==TM_USB_HIDHOST_Result_Disconnected)

{

for(i=0;i<4200000;i++)

GPIO_SetBits( GPIOD, GPIO_Pin_12);

for(i=0;i<4200000;i++)

GPIO_ResetBits( GPIOD, GPIO_Pin_12); }

} }

Thank you for helping me. 

#usb-otg #keyboard #usb-hid #stm32-usb #usb-host
0 REPLIES 0