cancel
Showing results for 
Search instead for 
Did you mean: 

Transmission of a matrix on CAN bus

ECiot.1
Associate II

Hi, I have an STM32H723ZG and I want to transmit a matrix in which I stored some measured data on a CAN bus. I can use the following function only writing the pointer to the matrix in "pTxData" or I have to segment the matrix?

HAL_FDCAN_AddMessageToTxFifoQ (FDCAN_HandleTypeDef * hfdcan,
FDCAN_TxHeaderTypeDef * pTxHeader, uint8_t * pTxData)

Moreover, I have to define manually the "pTxHeader" or is it created automatically by the STM32CubeMX?

1 REPLY 1
Karl Yamashita
Lead III

You can pass the pointer to the data. You have to create a new pTxHeader instance, then configure the pTxHeader with appropriate arguments.

Tips and Tricks with TimerCallback https://www.youtube.com/@eebykarl
If you find my solution useful, please click the Accept as Solution so others see the solution.