2019-05-08 8:30 AM
A bug in cubemx hal lib,a file named "stm32l4xx_hal_adc.h" in the STM32Cube_FW_L4_V1.13.0 ,in code line 518.#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_CH4) make sure as #define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_TRGO)
Solved! Go to Solution.
2019-05-09 12:59 AM
Hello,
This issue is fixed with the latest version of STM32CubeL4 V1.14.0.
#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_TRGO) /*!< ADC group regular conversion trigger from external peripheral: TIM4 TRGO. Trigger edge set to rising edge (default setting). */Please update and use this new version contains correction.
Regards,
Imen
2019-05-09 12:59 AM
Hello,
This issue is fixed with the latest version of STM32CubeL4 V1.14.0.
#define ADC_EXTERNALTRIG_T4_TRGO (LL_ADC_REG_TRIG_EXT_TIM4_TRGO) /*!< ADC group regular conversion trigger from external peripheral: TIM4 TRGO. Trigger edge set to rising edge (default setting). */Please update and use this new version contains correction.
Regards,
Imen