cancel
Showing results for 
Search instead for 
Did you mean: 

SVD file of the STM32H753 seems erronous compared to the stm32h753xx.h.

ZiggyS
Associate

The DFSDM section 29.7 channel configuration register has an offset for each channel of 0x20*y while the SVD file has a 0x4 offset between the channels. Can somebody state the correct offset?

SVD:

...

     <name>DFSDM_CHCFG0R1</name>

     <displayName>DFSDM_CHCFG0R1</displayName>

     <description>DFSDM channel configuration 0 register

     1</description>

     <addressOffset>0x0</addressOffset>

.....

     <name>DFSDM_CHCFG1R1</name>

     <displayName>DFSDM_CHCFG1R1</displayName>

     <description>DFSDM channel configuration 1 register

     1</description>

     <addressOffset>0x4</addressOffset>

.h

...

#define DFSDM1_Channel0_BASE (DFSDM1_BASE + 0x00)

#define DFSDM1_Channel1_BASE (DFSDM1_BASE + 0x20)

#define DFSDM1_Channel2_BASE (DFSDM1_BASE + 0x40)

#define DFSDM1_Channel3_BASE (DFSDM1_BASE + 0x60)

#define DFSDM1_Channel4_BASE (DFSDM1_BASE + 0x80)

#define DFSDM1_Channel5_BASE (DFSDM1_BASE + 0xA0)

#define DFSDM1_Channel6_BASE (DFSDM1_BASE + 0xC0)

#define DFSDM1_Channel7_BASE (DFSDM1_BASE + 0xE0)

-Z

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee

Hello @Sigbjørn Kolberg​ ,

You are right, the svd file is wrong.

We raised this issue internally for fix in the coming release.

Thanks for highlighting this issue.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
JHoll
Associate

Any signs of this fix coming soon? I'm porting code from an F4 to an H7 and really need to see what's happening in the DFSDM system.

Regards,

Jason

Imen.D
ST Employee

Hello,

Please find attached the updated STM32H753.svd file.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen