cancel
Showing results for 
Search instead for 
Did you mean: 

STN32H747 Dual Core - only reset 1 core

Joe.H
Senior

I can perform a software system reset but what I want to do is have the M7 reset the M4 cpu - is there a way?

I have always written my own bootloader so the product can have firmware upgraded in the field.

With the Dual Core - the M7 will be updating the flash memory space for the M4 and I need to be able to have it start back at its reset vector.

Thanks

4 REPLIES 4
Uwe Bonnes
Principal III

Try SCB_AIRCR_VECTRESET

Imen.D
ST Employee

Hello @Joe.H​ ,

Did you tried the line suggested by @Uwe Bonnes​  ? If his proposal works, please mark the reply as Best answer (click on "Select as Best").

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

If I read the documentation properly - it states that CPU1 can software reset CPU1 and CPU2 can software reset CPU2. I do NOT believe that it states CPU1 can reset CPU2 via that process.

If my statement is correct - than it does not answer the question.

Thanks for trying.

I did not notice your request to reset the other CPU. I scanned RM0399 and did also not find anything.