2018-03-21 5:27 AM
Hello there,
I am using the STM32L4 family MCU. In my hardware design, only after the USB cable is connected the voltage is applied to the VDD_USB pin of the MCU. At no USB connection this voltage is not present.
As a follow-up to this discussion, I am trying to configure everything now:
https://community.st.com/0D50X00009XkhQCSAZ
My problem consists of 2 sub-problems:
The procedure described in the datasheet is as follows:
What I do is the following:
In the generated code I see it is enabled:
/**
* Initializes the Global MSP. */void HAL_MspInit(void){ /* USER CODE BEGIN MspInit 0 *//* USER CODE END MspInit 0 */
__HAL_RCC_SYSCFG_CLK_ENABLE();
__HAL_RCC_PWR_CLK_ENABLE();HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* System interrupt init*/
/* MemoryManagement_IRQn interrupt configuration */ HAL_NVIC_SetPriority(MemoryManagement_IRQn, 0, 0); /* BusFault_IRQn interrupt configuration */ HAL_NVIC_SetPriority(BusFault_IRQn, 0, 0); /* UsageFault_IRQn interrupt configuration */ HAL_NVIC_SetPriority(UsageFault_IRQn, 0, 0); /* SVCall_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SVCall_IRQn, 0, 0); /* DebugMonitor_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DebugMonitor_IRQn, 0, 0); /* PendSV_IRQn interrupt configuration */ HAL_NVIC_SetPriority(PendSV_IRQn, 15, 0); /* SysTick_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0);/* Peripheral interrupt init */
/* PVD_PVM_IRQn interrupt configuration */ HAL_NVIC_SetPriority(PVD_PVM_IRQn, 5, 0); HAL_NVIC_EnableIRQ(PVD_PVM_IRQn);/* USER CODE BEGIN MspInit 1 */
/* USER CODE END MspInit 1 */
}2. I enable the PVM1:
/**
* @brief Enable the Power Voltage Monitoring 1: VDDUSB versus 1.2V. * @retval None */void HAL_PWREx_EnablePVM1(void){ SET_BIT(PWR->CR2, PWR_PVM_1); }3. Now I need to wait the ''PVM1 wakeup time'' but since I have no idea what is this time or I cant wait for the PVM1 interrupt as it doesnt work (I dont know why) I am stuck.
The PVM1 interrupt should work when I apply or remove voltage from VDD_USB if I understand correctly. For me it does not. Also the datasheet doesnt specify at any point what is the ''PVM1 wakeup time''.
When I use the debugger I see that the program acts as there is power (even though I do not supply it) but after I stop on the next line, I can see in the PWR_SR2 register that the flag is correct. It feels like its already to late when I stop with debugger and the flag changes...
As a prove, let me show you this case:
I have no USB cable connected, thus VDD_USB is near 0 V. This function returns ''true'':
bool usbds_isPowerPresent()
{ return (!HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_PVMO1));}Now, this modified version of the function returns false:
bool usbds_isPowerPresent()
{ volatile uint32_t dummy = HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_PVMO1); (void)dummy; return (!HAL_IS_BIT_SET(PWR->SR2, PWR_SR2_PVMO1));}This happends because there is more time between Enabling PVM1 and reading the register. But what is that time?
I would appreciate all help regarding this issue. Are there any additional steps I should take to make this work?
#usbSolved! Go to Solution.
2018-09-11 8:23 AM
In case anyone has a similar problem, here is the solution provided by ST:
Points 2 and 3 should be generated by CubeMX but are not. That was the problem.
2018-03-24 7:04 AM
Anyone please?
2018-03-24 8:23 AM
This isn't an effective conduit to ST support staff and FAE, perhaps it should be, so flag FAE Participation in your Community Survey submission.. I don't work for ST and am not paid by them, I get very little community support for my projects and work.
Are there no ST support engineers in the offices near you that you can cultivate a relationship with?
2018-03-24 8:28 AM
Thanks for answer,
Unfortunetaly there are none. I live in a poor country, forgotten by the world, with poor support for everything.
I will try to contact support.
2018-03-24 9:00 AM
Always considered Poland to be strong from a math/engineering perspective, although with the way the EU works at lot of the technical people immigrate to places where they are appreciated more. Ironically a lot end up in the UK, but I left there because the popular press, and population, seem to think engineers drive trains, install boilers or repair cars.
2018-03-24 9:13 AM
I can relate to your problem beoing i poland as well.
Anyways, I of course appreciate your help through all my years (in more than one company and also on ublox forums). Just dont have my own resources to pay you back.
I am just sitting here trying to make this device finally work.
2018-03-24 9:14 AM
>> I live in a poor country, forgotten by the world
Really? I live in the same country. The support is not for free.
2018-03-24 9:21 AM
Maybe this strenghes our position.
2018-09-11 8:23 AM
In case anyone has a similar problem, here is the solution provided by ST:
Points 2 and 3 should be generated by CubeMX but are not. That was the problem.