Skip to main content
marko239955_st
Associate
January 26, 2017
Question

MxCube USB library, how to send ACK trough Endpoint0 OUT

  • January 26, 2017
  • 1 reply
  • 628 views
Posted on January 26, 2017 at 14:16

Hi,

I am struggling to make a vendor device, that sends request on control pipe endpoint 0 out (EP0_OUT), I can receive the request correctly, but I can't send an ACK back (zero length packet). I have tried USBD_CtlSendData(), USBD_CtlSendStatus(),...the response doesn't seem to be sent anyway, neither on EP0_IN. 

I have other requests coming on EP0_IN and everything works correct.

I have been looking the library and had noticed, that any transmit request is parsed to be sent on EP0_IN

HAL_StatusTypeDef HAL_PCD_EP_Transmit(PCD_HandleTypeDef *hpcd, uint8_t ep_addr, uint8_t *pBuf, uint32_t len)

{

PCD_EPTypeDef *ep = NULL;

ep = &hpcd->IN_ep[ep_addr & 0x7F];

/*setup and start the Xfer */

ep->xfer_buff = pBuf;

ep->xfer_len = len;

ep->xfer_count = 0;

ep->is_in = 1;

ep->num = ep_addr & 0x7F;

HAL_PCD_EP_Transmit() calls USB_EPStartXfer, but before it sets ep->is_in=1, indicating to EP0_IN always.

USB_EPStartXfer then checks if it has to send to IN or OUT endpoint. 

HAL_StatusTypeDef USB_EPStartXfer(USB_TypeDef *USBx , USB_EPTypeDef *ep)

{

uint16_t pmabuffer = 0;

uint32_t len = ep->xfer_len;

/* IN endpoint */

if (ep->is_in == 1)

{

/*Multi packet transfer*/

if (ep->xfer_len > ep->maxpacket)

So, how could I send to EP0_OUT?

#stm32driver-usb
This topic has been closed for replies.

1 reply

rali717
Visitor II
September 10, 2018

I had the same issue,I guess.

After  I detect my vendor request,

I have to call this to receive the data.

USBD_CtlPrepareRx (pdev, myBuffer, sizeOfData)

That's do the trick for me.