cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h7s78-dk how to run FATfs Multi Access

ropodi17
Associate II

Hi Team,


I'm trying to run Fatfs Multi Access example in the stm32h7s78-dk. Im having hard time understanding the Readme instructions.  I have the switch set to boot0.

Im using stmcube progrmamer. I have added external loader: MX66UW1G45G_STM32H7S78-DK.stldr too then loaded the code. but it doesn't work. 

Am I missing something? What should I do with 

Template_XIP_Boot.hex file? A clear step by step intructions would be great


Thank you
Rohit
2 REPLIES 2
MOBEJ
ST Employee

Hello @ropodi17 , 

To ensure the program functions correctly, follow these steps using STM32CubeIDE: 

  • Compile the example/application; the elf file is required to configure the debug profile (the “active configuration” must be “debug”, else only assembly debug is available)
  • Open the menu [Run]->[Debug configuration] and double click on [STM32 C/C++ Application] (it creates a default debug configuration for the current project selected)
  • In [Debugger] tab, section “External loaders” add the external loader corresponding to your Board/Memory as described below:
  • In “External loaders” section, click on [Add]
  • Select the loader among the available list (MX25UW25645G_NUCLEO-H7S3L8.stldr or MX66UW1G45G_STM32H7S78-DK.stldr)
  • Option “Enabled” checked and Option “Initialize” unchecked
  • In “Misc” section, uncheck the option “Verify flash download”
  • In [Startup] tab, section “Load Image and Symbols”:
    • Click on [Add]
    • If your project contains a boot project:
      • click on “Project” and then select the boot project.
      • click on Build configuration and select “Use active”.
      • then select the following options:
        • “Perform build” checked.
        • “Download” checked.
        • “Load symbols” unchecked.
    • If your project doesn’t contain a boot project:
      • click on [File System] and select the Boot HEX file corresponding to your board

        Boot_XIP.hex can be found in folder [Binary] on each Template_XIP project

        You may need to force the capability to select a .hex file by typing " * " + pressing the “Enter” key in the file name dialog

      • then select the following options:
        • “Download” checked.
        • “Load symbols” unchecked.
        • Click Ok
      • Back in the in the [Startup] tab, move down the boot project for it to be in second position
  • Our debug configuration is ready to be used.

Thank you, and I hope this helps!

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @MOBEJ ,

 

Thanks for the detailed steps in STM32cubeIDE, 
Actually I would like to know how to program the board using STM32CUBE Programmer. To program it permanently.

Thanks