STM32H753 USB Host pin not reseted to original state when stopping driver
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-14 3:15 AM
STM32H753
HAL 1.19.1
I need to reset the USB host dedicated pins (PB14/PB15) to their original state when stoping the USB HOST driver.
The USB Host driver is activated on demand using MX_USB_HOST_init.
The HS part is activated and the driver is well performing.
Once the USB Host task has processed its data, I need to stop it.
I then call USBH_DeInit and USBH_LL_Deinit, so the HAL_HCD_MspDeInit is called and the USB Host pins are reconfigured so they are not used for USB AF anymore.
Mesuring voltage the PB14/PB15 pins, they doesn't return to their original state.
Original state : PB14/PB15 2.5V/2.5V
After usb usage : PB14/PB15 3.3V/0.5V
Any advice ?
- Labels:
-
STM32H7 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-14 6:18 AM
For someone who would have the same problem :
Just after USBH_DeInit and USBH_LL_Deinit add :
/* Deactivate the USB Transceiver */
__HAL_RCC_USB_OTG_HS_CLK_ENABLE();
((HCD_HandleTypeDef *)hUsbHostHS.pData)->Instance->GCCFG &= ~(USB_OTG_GCCFG_PWRDWN);
__HAL_RCC_USB_OTG_HS_CLK_DISABLE();
That is, powerdown the USB PHY (HS).
And the voltage will return to initial state and the pins will be available for something else.
Cheers !
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-14 6:18 AM
Look at the GPIOB registers to verify they are configured as you wish.
If they are not, add the appropriate (de)initialization in HAL_HCD_MspDeInit.