cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745 SDMMC block reads returning empty

Matt__
Associate II

Hello, 

I am working on trying to get the SDMMC1 on the stm32h745 to function properly. Currently I have this for my current initialization of the SDMMC and it does not return any errors. 

hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B; 
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 0;

if (HAL_SD_Init(&hsd1) != HAL_OK) {
Error_Handler();
}
if (HAL_SD_ConfigWideBusOperation(&hsd1, SDMMC_BUS_WIDE_4B) != HAL_OK) {
Error_Handler();
}

 

After this is done, I try to use the HAL_SD_ReadBlocks_IT(); and also this does not return any errors. The issue I am having is the return data buffer has no data in it when this function finishes. Currently I am not sure what the issue might be, the clocks and appear as they are sending data but I am getting nothing in my return data. Any thoughts or ideas on what might resolve this problem? 

Thanks 

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

I have tried using medium to very high and not found a difference in the speed I increase the clock. The series resistors are 220 ohms and the pull up resistors are 47.5k.

220 is too much - try 51 or 33 . And medium or hi speed . And 1 bit mode.

If you feel a post has answered your question, please click "Accept as Solution".

Actually the series resistor is 22ohm, sorry i misread when looking.