cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H723ZGT6 with LAN8720A Ethernet PHY

132416541
Associate

phy芯片设置百兆全双工自协商连接千兆交换机时网络ping不通,连接百兆交换机正常 P1连接千兆交换机phy寄存器 P2连接百兆交换机寄存器 P3主控关键寄存器

Translation:

When the Ethernet PHY chip is set to 100M full-duplex auto-negotiation and connected to a gigabit switch, the network ping fails, but it works normally when connected to a 100M switch. P1 connects to the gigabit switch phy register. P2 connects to the 100M switch register. P3 master control key register.

132416541_1-1745218655963.png

132416541_2-1745218665245.png132416541_3-1745218679124.png

 

 

 

 

 

1 REPLY 1
ASEHST
ST Employee

Hello @132416541,

Thank you for your report.

It appears that the auto-negotiation is failing to establish the correct connection despite being enabled on both sides, on the LAN8720 and the switch.

To better understand and resolve your problem, could you please provide us with more information about your switches, specifically their reference and whether they are manageable or not? This will help us identify any configuration settings that might need adjustment to improve compatibility.

 

With Regards,

If your question is answered, please close this topic by clicking "Accept as Solution".