2026-05-07 1:19 AM - last edited on 2026-05-07 1:43 AM by mƎALLEm
Hi Community,
I'm a new Developer/ for ST Microcontrollers, Now Im currently using STM32H723ZGT6 (NUCLEO - 144). Im currently working on ethernet (LWIP), the ping is not working for this code that i have generated . I have seen some youtube channels but I cant rectify and make the ping, I have tried all the possible things like , flash linker script , enabling ICache , Dcache , using MPU(Memory Protection Unit), change them to static ip for both board and my PC and So on . I have tried but I dont know whether my code or my implementation is correct or not . Can anybody help me with this ?..
I have attached the file thats my code and how project. pls have a look into that.
Thank You.
2026-05-07 1:44 AM
Hello @Gokul_Sarvanakumar_60 and welcome to the ST community,
How to create a project for STM32H7 with Ethernet and LwIP stack working
2026-05-07 4:31 AM
Thank You for the reply still its not working, I cant identify the issue.
2026-05-07 6:20 AM
I'm almost sure you didn't follow the exact steps described in the knowledge base article.
2026-05-07 7:23 AM - edited 2026-05-07 7:24 AM
Do these ready, pre-configured examples work for you?
2026-05-07 9:21 PM
yes these pre- configured are perfectly working. but my own code is not working
2026-05-10 8:34 PM
can we do IP config without Free RTos , if possible pls share me a precofigured code , so that i can compare with my code and understand the error
2026-05-10 11:17 PM - edited 2026-05-10 11:19 PM
2026-05-11 12:31 AM - edited 2026-05-11 12:34 AM
Here you can find preconfigured LwIP examples without RTOS: LwIP_TCP_Echo_Server, LwIP_UDP_Echo_Server
Also you may want to try Mongoose https://mongoose.ws/wizard/#/
2026-05-11 2:06 AM
Hi @Pavel A. , Thanks for your continuous support and reply, yet still i cant figure it out . all the preconfigured is running but i cant remake it on my own , if possible , I am ready to have a one on one conversation with you. anything through G meet or Team or even im ready to give my personal mobile number. my personal mail : gokulsha990@gmail.com