2025-04-23 12:39 AM
When using the register callbacks feature ( USE_HAL_UART_REGISTER_CALLBACKS = 1) , the BSP does not register the default callback, causing the serial port not to work.
Fix:
diff --git a/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c b/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c
index 89b0837..bd2dd97 100644
--- a/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c
+++ b/Drivers/BSP/STM32G4xx_Nucleo/stm32g4xx_nucleo.c
@@ -384,7 +384,7 @@ int32_t BSP_COM_Init(COM_TypeDef COM, COM_InitTypeDef *COM_Init)
/* Init the UART Msp */
COM1_MspInit(&hcom_uart[COM]);
#else
- if(IsComMspCbValid == 0U)
+ if(IsComMspCbValid[COM] == 0U)
{
if(BSP_COM_RegisterDefaultMspCallbacks(COM) != BSP_ERROR_NONE)
{Solved! Go to Solution.
2025-04-24 2:17 AM
Hello @lamare ,
Issue reported. Internal Ticket 208444 (not accessible by community users).
2025-04-23 3:07 AM
Hi @lamare
Do you configured the uart interrupt line and Nvic ?
2025-04-24 12:20 AM
There's an obvious bug in the stm32g4xx_nucleo.c file. At line 96 there's the declaration of the IsComMspCbValid array:
static uint32_t IsComMspCbValid[COMn] = {0};#if (USE_HAL_UART_REGISTER_CALLBACKS == 0)
/* Init the UART Msp */
COM1_MspInit(&hcom_uart[COM]);
#else
if(IsComMspCbValid == 0U)
{
if(BSP_COM_RegisterDefaultMspCallbacks(COM) != BSP_ERROR_NONE)
{
return BSP_ERROR_MSP_FAILURE;
}
}
#endifSince IsComMspCbValid is a static array that has an address, this if statement:
if(IsComMspCbValid == 0U)is *always* false, so BSP_COM_RegisterDefaultMspCallbacks is never called.
So, the if statement should be:
if(IsComMspCbValid[COM] == 0U)
This way, it checks the value at offset COM in the array....
2025-04-24 2:17 AM
Hello @lamare ,
Issue reported. Internal Ticket 208444 (not accessible by community users).