2020-07-27 2:03 AM
Hi,
in my Project i am using the STM32H743VI processor in a custom board design. My CubeMX configuration is attached. The problem is that after i configure the USB_DEVICE stack in CubeMX and generate the Code i can not anymore connect to the board over TCP/IP. Before the configuration of the USB_DEVICE stack i was able to communicate and connect to the board over tcp/ip. Also when i reconfugure the CubeMX project and disable the USB_DEVICE it isn't possible to connect over tcp/ip. The only solution is to make a completely new project. I verified all the electrical connections of my board. There are no problems.
I attached the CubeMX project with the configured USB_DEVICE and LWIP stack and my main source code.
Thanks in advance.