2023-01-23 8:28 AM
Using STM32 HAL and a STM32H7 (I know some dissuade the usage of this). I have created 2 MPU Regions of non cacheable memory .
void MPU_Config(void) {
MPU_Region_InitTypeDef MPU_InitStruct = { 0 };
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x24060000;
MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;
MPU_InitStruct.SubRegionDisable = 0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0x240E0000;
MPU_InitStruct.Size = MPU_REGION_SIZE_128KB;
MPU_InitStruct.SubRegionDisable = 0x0;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_HFNMI_PRIVDEF);
}
and created a loader:
MEMORY
{
...
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 384K
RAM_NOCACHE (xrw) : ORIGIN = 0x24060000, LENGTH = 1024K - 384K
...
}
...
.DATA_RAM_NOCACHE (NOLOAD) :
{ . = ALIGN(4);
*(.DATA_RAM_NOCACHE)
*(.DATA_RAM_NOCACHE*)
. = ALIGN(4);
} >RAM_NOCACHE When using memory of just 512Kb with 1 MPU area defined things work as expected but a Hard Fault occurs when I try the above - a memory alignment error - more details to follow...)
Is this because there are 2 regions. How can it be done thanks
Solved! Go to Solution.
2023-01-23 12:09 PM
> MPU_InitStruct.BaseAddress = 0x24060000;
> MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;
Base address of a region must be aligned on the region size.
2023-01-23 8:35 AM
empty
2023-01-23 12:09 PM
> MPU_InitStruct.BaseAddress = 0x24060000;
> MPU_InitStruct.Size = MPU_REGION_SIZE_512KB;
Base address of a region must be aligned on the region size.
2023-01-23 12:26 PM
Does that mean that starting at 0x24060000 - 3 * 256Kb areas should be assigned?
> MPU_InitStruct.Number = MPU_REGION_NUMBER0;
> MPU_InitStruct.BaseAddress = 0x24060000;
> MPU_InitStruct.Size = MPU_REGION_SIZE_256KB;
> MPU_InitStruct.Number = MPU_REGION_NUMBER1;
> MPU_InitStruct.BaseAddress = 0x240A0000;
> MPU_InitStruct.Size = MPU_REGION_SIZE_256KB;
> MPU_InitStruct.Number = MPU_REGION_NUMBER2;
> MPU_InitStruct.BaseAddress = 0x240E0000;
> MPU_InitStruct.Size = MPU_REGION_SIZE_256KB;
Does that mean that starting at 0x24060000 - a 1 * 128Kb area ?
and at at 0x24080000 a 1 * 512Kb region?
Obvs tried it and bingo!
Works a charm. Thank you