cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H573: ETH SWRESET fails, ETH_DMAMR_SWR stays set, timeout

Lionheart1810
Visitor

I want to initialize the STM32H573 ETH module using the STM32CubeMX code generator (see ioc file attached). It should run in MII mode using an external transceiver.

I kept the configuration unchanged, however it always jumps to ErrorHandler, because HAL_ETH_Init returns HAL_ERROR on timeout of ETH_DMAMR_SWR at the following routine:

  SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR);

  /* Get tick */
  tickstart = HAL_GetTick();

  /* Wait for software reset */
  while (READ_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR) > 0U)
  {
    if (((HAL_GetTick() - tickstart) > ETH_SWRESET_TIMEOUT))
    {
      /* Set Error Code */
      heth->ErrorCode = HAL_ETH_ERROR_TIMEOUT;
      /* Set State as Error */
      heth->gState = HAL_ETH_STATE_ERROR;
      /* Return Error */
      return HAL_ERROR;
    }
  }

From what I've read on this forum, the ETH somehow needs an external clock input from the transceiver. However, ETH_REF_CLK is only defined in RMII mode, but I want MII mode with RX and TX clocks. Does it still need permanently running clock? ETH_RX_CLK is currently served from the transceiver with 2.5 MHz (in 10 Mbps mode), the ETH module itself is clocked 100 MHz from PLL1Q:

Screenshot_20250203_191600.png

I even tried rising the timeout threshold, but even 50 s is failing. Any ideas on how to get the initialization through?

1 REPLY 1
alister
Lead

ETH_REF_CLK is for RMII. ETH_RX_CLK and ETH_TX_CLK are for MII.

I observed HAL_ETH_Init failing similarly for the STM32H7S78-DK last year and posted that and a fix at https://community.st.com/t5/stm32cubemx-mcus/bugs-caveats-misc-fixes-stm32h7s-cube/td-p/710992. For clarity, the peripheral clock's fix in HAL_ETH_MspInit was:

 

 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ETH1REF;
 PeriphClkInit.Eth1RefClockSelection = RCC_ETH1REFCLKSOURCE_PHY;