2024-11-27 4:28 AM
ADC_CFGR register and EXTSEL field.
In SVD this single field is split among four 1-bit long ones (according to RM0492) and enumerated values desciptions are messed up (adc_ext_trg0 & adc_ext_trg1 repeated for all 4 "subfields")
RM0492 discusses this as single field, which is correct, i.e.
"Bits 9:5 EXTSEL[4:0]: External trigger selection for regular group
These bits select the external event used to trigger the start of conversion of a regular group:
00000: adc_ext_trg0
00001: adc_ext_trg1
00010: adc_ext_trg2
00011: adc_ext_trg3
00100: adc_ext_trg4
00101: adc_ext_trg5
00110: adc_ext_trg6
00111: adc_ext_trg7
...
11111: adc_ext_trg31"
etc...
In the same time ADC_JSQR_JEXTSEL is defined as single 5-bit long field.
Bits 6:2 JEXTSEL[4:0]: External Trigger Selection for injected group
Logical inconsistecy...
Is SVD created from RM or vice versa?
Either way I think RM0492 (page 579), SVD and stm32h503xx.h files shall be corrected, to have both descriptions, i.e. EXTSEL & JEXTSEL aligned.
2024-11-27 7:16 AM
Hello @hijax_pl,
Thank you again for having reported the point related to SVD issue.
I escalated this request internally for fix within the internal ticket number: 197196 (this tracking number is only for reference, not available outside of ST).
2024-12-23 5:14 AM
Hello @hijax_pl ,
The fix has been applied to the SVD files for STM32H5.
The new SVD files are available in the attached file.